之前有朋友用过2407和2812,I/O口输入接74LS14的输出5V电压都没有问题,可是我在文档上没有看到相关的说明,如果有相关文档能否提供给我?!另外我现在要用28335,输入口不知道能否外接74LS14的输出,带有相关说明的文档也请提供给我,希望给予我支持,谢谢啊!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前有朋友用过2407和2812,I/O口输入接74LS14的输出5V电压都没有问题,可是我在文档上没有看到相关的说明,如果有相关文档能否提供给我?!另外我现在要用28335,输入口不知道能否外接74LS14的输出,带有相关说明的文档也请提供给我,希望给予我支持,谢谢啊!
楼主你好!
F28335I/O口是不能支持5V的,因此,如果要输入、输出5V的话,请接电平转换IC或者相应电路。楼主可以看74LS14的规格书,输出高电平的典型值为3.4V。而不是5V。
感谢回答,此问题解决。另有一问题,TPS767D301PWP是5V输入双路3.3和可调输出,我想用他做28335供电电源,看资料发现它属于LDO,5V-1.9V压差也很大,而且28335在150MHZ时候有400mA电流,这样一计算就有1.2W的功率,那么这个LDO 就会很热,然而TI之所以推荐这款说是因为很多人用这个芯片作为28335电源芯片,我希望知道这款是不是最优选择,如果不是,请帮我推荐一款5V输入1.9V可调输出,1A负载能力的单路电源芯片,要常用,性价比高的,感谢支持!