This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
// This program requires the f2802x header files.
//
// Make sure the CPU clock speed is properly defined in
// f2802x_Examples.h before compiling this example.
// Description:
//
// This example sets up the PLL in x12/2 mode.
//
// For 60 MHz devices (default)
// (assuming a 10Mhz input clock).
//
// Interrupts are enabled and the ePWM1 is set up to generate a periodic
// ADC SOC interrupt - ADCINT1. One channel is converted - ADCINA5, which is
// internally connected to the temperature sensor.
//
// Watch Variables:
//
// TempSensorVoltage[10] Last 10 ADCRESULT0 values
// ConversionCount Current result number 0-9
// LoopCount Idle loop counter
//
//
//###########################################################################
// $TI Release: F2802x Support Library v230 $
// $Release Date: Fri May 8 07:43:05 CDT 2015 $
// $Copyright: Copyright (C) 2008-2015 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
// Prototype statements for functions found within this file.
__interrupt void adc_isr(void);
// Global variables used in this example:
uint16_t LoopCount;
uint16_t ConversionCount;
uint16_t TempSensorVoltage[10];
void main()
{
// WARNING: Always ensure you call memcpy before running any functions from RAM
// InitSysCtrl includes a call to a RAM based function and without a call to
// memcpy first, the processor will go "into the weeds"
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the f2802x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initialize GPIO:
// This example function is found in the f2802x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the f2802x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in f2802x_DefaultIsr.c.
// This function is found in f2802x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected register
PieVectTable.ADCINT1 = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
// Step 4. Initialize the ADC:
// This function is found in f2802x_Adc.c
InitAdc(); // For this example, init the ADC
AdcOffsetSelfCal();
// Step 5. Configure ADC to sample the temperature sensor on ADCIN5:
// The output of Piccolo temperature sensor can be internally connected to the ADC through ADCINA5
// via the TEMPCONV bit in the ADCCTL1 register. When this bit is set, any voltage applied to the external
// ADCIN5 pin is ignored.
EALLOW;
AdcRegs.ADCCTL1.bit.TEMPCONV = 1; //Connect internal temp sensor to channel ADCINA5.
EDIS;
// Step 6. Continue configuring ADC to sample the temperature sensor on ADCIN5:
// Since the temperature sensor is connected to ADCIN5, configure the ADC to sample channel ADCIN5
// as well as the ADC SOC trigger and ADCINTs preferred. This example uses EPWM1A to trigger the ADC
// to start a conversion and trips ADCINT1 at the end of the conversion.
//Note: The temperature sensor will be double sampled to apply the workaround for rev0 silicon errata for the ADC 1st sample issue
EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch
AdcRegs.INTSEL1N2.bit.INT1E = 1; //Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; //Disable ADCINT1 Continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 1; //setup EOC1 to trigger ADCINT1 to fire
AdcRegs.ADCSOC0CTL.bit.CHSEL = 5; //set SOC0 channel select to ADCINA5 (which is internally connected to the temperature sensor)
AdcRegs.ADCSOC1CTL.bit.CHSEL = 5; //set SOC1 channel select to ADCINA5 (which is internally connected to the temperature sensor) errata workaround
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 5; //set SOC0 start trigger on EPWM1A
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 5; //set SOC1 start trigger on EPWM1A errata workaround
AdcRegs.ADCSOC0CTL.bit.ACQPS = 36; //set SOC0 S/H Window to 37 ADC Clock Cycles, (36 ACQPS plus 1)
AdcRegs.ADCSOC1CTL.bit.ACQPS = 36; //set SOC1 S/H Window to 37 ADC Clock Cycles, (36 ACQPS plus 1) errata workaround
EDIS;
// Step 7. User specific code, enable interrupts:
// Enable ADCINT1 in PIE
PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE
IER |= M_INT1; // Enable CPU Interrupt 1
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
LoopCount = 0;
ConversionCount = 0;
// Assumes ePWM1 clock is already enabled in InitSysCtrl();
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm1Regs.CMPA.half.CMPA = 0x0080; // Set compare A value
EPwm1Regs.TBPRD = 0xFFFF; // Set period for ePWM1
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // count up and start
// Wait for ADC interrupt
for(;;)
{
LoopCount++;
}
}
__interrupt void adc_isr(void)
{
TempSensorVoltage[ConversionCount] = AdcResult.ADCRESULT1; //discard ADCRESULT0 as part of the workaround to the 1st sample errata for rev0
// If 20 conversions have been logged, start over
if(ConversionCount == 9)
{
ConversionCount = 0;
}
else
{
ConversionCount++;
}
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Clear ADCINT1 flag reinitialize for next SOC
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
return;
}