我采用的ccs版本是Version: 6.1.1.00022 ,芯片是28377,用c2prog串口烧写程序总是有问题,应该是ccs输出hex文件有问题,设置不正确。请问这块如何设置?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我采用的ccs版本是Version: 6.1.1.00022 ,芯片是28377,用c2prog串口烧写程序总是有问题,应该是ccs输出hex文件有问题,设置不正确。请问这块如何设置?
请问具体是什么错误呢?
需要注意的是在general optional中设置
--memwidth=16 --romwidth=16 --intel
This means that your hex-file contains data that does not fall into a valid flash sector. Please double-check your linker command file and make sure that only flash data is linked to page 0.
链接: http://www.codeskin.com/c2prog-faq
应该是您的.hex文件或是.out文件本身或是转换时出现了问题
一般是因为在hex文件的第一行出现了不是在flash扇区地址,将hex文件的第一行删掉试一下
解决了啊,就是选择intel 模式即可,你照做了没有呢?