您好:
我在使用F28035操作AT24C04的时候,发现一个问题,就是写EEPROM之后,立刻读取EEPROM内容,使用查询方式的时候,I2C状态寄存器会没有反应,例如
I2caRegs.I2CMDR.all = 0x2620; // Send data to setup EEPROM address
执行之后,如果我查询ARDY标志位,发现没有反应,也就是说,ARDY没有设置为1,不知道是不是写法的问题,参考手册说,只要完成,就立刻给信号,但确实没给出,死在for循环里面了。
for(;;) { tmp++; if (I2caRegs.I2CSTR.bit.ARDY == 1) { if(I2caRegs.I2CSTR.bit.NACK == 1) { I2caRegs.I2CMDR.bit.STP = 1; I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT; I2caRegs.I2CFFTX.bit.TXFFRST = 0; I2caRegs.I2CFFTX.bit.TXFFRST = 1; flag = 0xff; } else { I2caRegs.I2CCNT = 1; // Setup how many bytes to expect I2caRegs.I2CMDR.all = 0x2C20; // Send restart as master receiver } break; }
}