This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问专家:
1、通过通讯接口传输程序进行Flash API烧写时,需要接收、解析程序保证待烧写程序长度能够放在CMD规定的一个FLASH段内吗?如果不检查长度,烧写后的程序超出了规定FLASH空间,会造成什么问题?
2、常规的FLASH段A-H是固化的吗?是否可以定制段的划分?如果定制,除了修改CMD还需要注意什么吗?
3、DSP运行的IAP和上位传输软件都自己编写时,推荐使用什么数据格式进行程序传输?
IAP的话,C2000 controlSUITE 您可以看一下
以及
c:\TI\c2000\C2000Ware_1_00_04_00\device_support\f2833x\examples\f28335_flash_kernel\
- SCI_Boot.c
- Share_Boot.c