This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28069 的XRS 为什么一直是低电平?



F28069 的XRS 为什么一直是低电平? 换了一片新的,还是一样

1.请检查你的3.3V供电驱动能是多少?     5V直流电源+3.3V的1117 供电应该没问题

2.请用直流源供3.3V测一下此时3.3V上有多大电流?------电池很小,芯片也不发热

3.还有就是检查有没有什么管脚的输入信号超过了3.3V。------------所有引脚没有超过3.3V

4.检查一下芯片焊接有没有出现管脚开路或者短路现象。-------------管脚开路,不用的AD引脚是开路的,(没有用到引脚,要怎样处理)

还有什么地方导致XRS脚一直是低电平呢?

使用内部VREGENZ 接地,VDD 2V