TI E2E™ 设计支持论坛将于 5 月 30 日至 6 月 1 日进行维护。如果您在此期间需要技术支持,请联系 TI 的客户支持中心寻求帮助。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP SCI FIFO 上位机通信

想通过FIFO,把数组Uint16 dataA={123,123,123,123,123,123,123,123}发送到上位机,FIFO是一次发送8个数据,分别是dataA的8个元素,但用串口助手看到的是123的ASC码{;

如果考虑用itoa转成字符串,此时char* msg={1,2,3},就很棘手了,怎么用FIFO一次发送8个123啊?

  • 请问您现在使用的是哪款芯片?若是可以的话请给出相关代码,谢谢
  • 您好,我使用的是28335,部分代码如下,我现在并不知道该怎么写我想实现的这个功能

    #include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
    #include "DSP2833x_Examples.h" // DSP2833x Examples Include File

    #define LED4 GpioDataRegs.GPADAT.bit.GPIO0
    #define LED3 GpioDataRegs.GPADAT.bit.GPIO1
    #define LED1 GpioDataRegs.GPADAT.bit.GPIO6
    #define LED2 GpioDataRegs.GPADAT.bit.GPIO7

    interrupt void ISRTimer0(void);
    void configtestled(void);

    void InitScibGpio();
    void Scib_Init(void);
    void Scib_Fifo_Init(void);
    interrupt void Scib_Tx_Isr(void);
    interrupt void Scib_Rx_Isr(void);
    void itoa(int num,char* str,int radix);

    Uint16 i = 0;
    Uint16 k = 123;
    Uint16 dataB[8];
    Uint16 dataA[3] = {1,2,3};
    char* msg;

    void main(void)
    {
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the DSP2833x_SysCtrl.c file.
    InitSysCtrl();

    // Step 2. Initalize GPIO:
    // This example function is found in the DSP2833x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    // InitGpio(); // Skipped for this example
    InitXintf16Gpio(); //zq

    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    DINT;

    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the DSP2833x_PieCtrl.c file.
    InitPieCtrl();

    // Disable CPU interrupts and clear all CPU interrupt flags:
    IER = 0x0000;
    IFR = 0x0000;

    // PIE 向量表指针指向中断服务程(ISR)完成其初始化.
    // 即使在程序里不需要使用中断功能,也要对 PIE 向量表进行初始化.
    // 这样做是为了避免PIE引起的错误.
    // The shell ISR routines are found in DSP2833x_DefaultIsr.c.
    // This function is found in DSP2833x_PieVect.c.
    InitPieVectTable();

    InitScibGpio();

    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    EALLOW; // This is needed to write to EALLOW protected registers
    PieVectTable.TINT0 = &ISRTimer0;
    PieVectTable.SCITXINTB = &Scib_Tx_Isr;
    PieVectTable.SCIRXINTB = &Scib_Rx_Isr;
    //PieVectTable.XINT13 = &cpu_timer1_isr;
    //PieVectTable.TINT2 = &cpu_timer2_isr;
    EDIS; // This is needed to disable write to EALLOW protected registers

    // Step 4. Initialize the Device Peripheral. This function can be
    // found in DSP2833x_CpuTimers.c
    InitCpuTimers(); // For this example, only initialize the Cpu Timers

    // Configure CPU-Timer 0, 1, and 2 to interrupt every second:
    // 150MHz CPU Freq, 1 second Period (in uSeconds)

    ConfigCpuTimer(&CpuTimer0, 150, 500000);
    //ConfigCpuTimer(&CpuTimer1, 150, 1000000);
    //ConfigCpuTimer(&CpuTimer2, 150, 1000000);
    //StartCpuTimer0();

    // Enable CPU int1 which is connected to CPU-Timer 0, CPU int13
    // which is connected to CPU-Timer 1, and CPU int 14, which is connected
    // to CPU-Timer 2:
    IER |= M_INT1;
    IER |= M_INT9;
    //IER |= M_INT13;
    //IER |= M_INT14;
    GpioDataRegs.GPBSET.bit.GPIO60=1;
    // Enable TINT0 in the PIE: Group 1 interrupt 7
    PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
    PieCtrlRegs.PIEIER1.bit.INTx7 = 1;

    PieCtrlRegs.PIEIER9.bit.INTx3 = 1;
    PieCtrlRegs.PIEIER9.bit.INTx4 = 1;

    // Enable global Interrupts and higher priority real-time debug events:
    EINT; // 总中断 INTM 使能
    ERTM; // 使能总实时中断 DBGM

    Scib_Init(); // Initalize SCIB
    Scib_Fifo_Init();

    configtestled();
    LED1=1;
    DELAY_US(10);
    LED2=1;
    DELAY_US(10);
    LED3=0;
    DELAY_US(10);
    LED4=0;
    DELAY_US(10);
    for(; ;);
    }

    interrupt void ISRTimer0(void)
    {
    // Acknowledge this interrupt to receive more interrupts from group 1
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; //0x0001赋给12组中断ACKnowledge寄存器,对其全部清除,不接受其他中断
    CpuTimer0Regs.TCR.bit.TIF=1; // 定时到了指定时间,标志位置位,清除标志
    CpuTimer0Regs.TCR.bit.TRB=1; // 重载Timer0的定时数据
    LED1=~LED1;
    LED2=~LED2;
    LED3=~LED3;
    LED4=~LED4;

    for(i=0; i<8; i++)
    {
    dataB[i]= k;
    }

    ScibRegs.SCIFFTX.bit.TXFIFOXRESET = 1; // 复位发送 FIFO 指针
    ScibRegs.SCIFFTX.bit.TXFFINTCLR = 1;


    }

    void Scib_Init()
    {
    ScibRegs.SCICCR.all = 0x0007;
    ScibRegs.SCICTL1.all = 0x0003;

    ScibRegs.SCICTL2.bit.TXINTENA = 1;
    ScibRegs.SCICTL2.bit.RXBKINTENA = 1;

    ScibRegs.SCIHBAUD = 0x0001; // 9600 baud @LSPCLK = 37.5MHz
    ScibRegs.SCILBAUD = 0x00E7;

    ScibRegs.SCICCR.bit.LOOPBKENA = 0; //Disable Loopback

    }

    void Scib_Fifo_Init()
    {
    //ScibRegs.SCIFFTX.bit.SCIRST = 1;
    ScibRegs.SCIFFTX.bit.TXFIFOXRESET = 1;
    ScibRegs.SCIFFTX.bit.SCIFFENA = 1;
    ScibRegs.SCIFFTX.bit.TXFFST = 0;
    ScibRegs.SCIFFTX.bit.TXFFINT = 0;
    ScibRegs.SCIFFTX.bit.TXFFINTCLR = 0;
    ScibRegs.SCIFFTX.bit.TXFFIENA = 1;
    ScibRegs.SCIFFTX.bit.TXFFIL = 0;

    ScibRegs.SCIFFRX.bit.RXFFOVF = 1;
    ScibRegs.SCIFFRX.bit.RXFFOVRCLR = 1;
    ScibRegs.SCIFFRX.bit.RXFIFORESET = 1;
    ScibRegs.SCIFFRX.bit.RXFFST = 0;
    ScibRegs.SCIFFRX.bit.RXFFINT = 0;
    ScibRegs.SCIFFRX.bit.RXFFINTCLR = 1;
    ScibRegs.SCIFFRX.bit.RXFFIENA = 1;
    ScibRegs.SCIFFRX.bit.RXFFIL = 3;

    ScibRegs.SCIFFCT.all = 0x00;
    ScibRegs.SCICTL1.all = 0x0023;
    ScibRegs.SCICTL1.bit.SWRESET = 1;
    }

    interrupt void Scib_Tx_Isr(void)
    {
    Uint16 i;
    for(i=0; i<8; i++)
    {
    itoa(dataB,msg,10);
    ScibRegs.SCITXBUF = msg[i];
    }
    PieCtrlRegs.PIEACK.all |= PIEACK_GROUP9;

    }

  • 请问,您有什么解决办法可以提出吗?