This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28035的SCI示例



在SCI模块官方示例中(loopback模式,无中断):

SCI的初始化scia_loopback_init函数中:

 SciaRegs.SCICTL2.all =0x0003;

 SciaRegs.SCICTL2.bit.TXINTENA      =1;

 SciaRegs.SCICTL2.bit.RXBKINTENA =1;

为什么这里SCICTL2要初始化2遍?  在SCICTL2.all=0x0003中已经完成了TXINTENA和RXINTENA的置位,不是重复了么?

另外本实例中没有使用接收中断,为什么要设置SciaRegs.SCIFFRX.all=0x2044?

 

  • Lzh,

           “为什么这里SCICTL2要初始化2遍?  在SCICTL2.all=0x0003中已经完成了TXINTENA和RXINTENA的置位,不是重复了么?”

            是重复了,可以comment掉。      

            “另外本实例中没有使用接收中断,为什么要设置SciaRegs.SCIFFRX.all=0x2044?”

             可以不用设置,对该例程没有影响。这里这么设计的原因应该是该例程是由使用接收中断的例程修改而来的,保留了这些配置。

    Eric