目前使用280049C LaunchPad kit
連接線是包裝內的 USB micro-B plug to USB-A plug cable
電腦環境為macOS
IDE環境為CCS Version: 8.3.1.00004
Target Configuration test connection:
The JTAG DR Integrity scan-test has succeeded.
進入DEBUG則出現以下錯誤訊息:
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 8.1.0.00012)