This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DRV8301 and DRV8302 High Current Three-Phase Brushless Motor Control Kits



        网上查SUM110N06-3m9H最大可通过110A电流,为什么在Main features中

  • Piccolo F28035 controlCARD with onboard isolated USB JTAG emulation
  • DRV830x 3-phase Integrated Motor Pre-Driver Evaluation Board
  • 60A FETS
  • NO POWER SUPPLY: 8-60V Supported
  • NO MOTOR INCLUDED: Spin YOUR motor with InstaSPIN™-BLDC
  • GUI, Detailed example software and documentation
  • Complete hardware schematics, gerber files, and BOM

这不限制了可连接到演示板上的电机的功率?   因为我想接个大一点功率的电机,请问这个板子最大能接多大功率的电机??