This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有关28069 GPIO 设置问题



GpioCtrlRegs.GPAMUX2.bit.GPIO18=0;//引脚功能:GPIO

NOP;
//(1)上拉
GpioCtrlRegs.GPAPUD.bit.GPIO18=0;//led上拉使能

NOP;
//(2)方向
GpioCtrlRegs.GPADIR.bit.GPIO18=1;//led 输出

NOP;
//(3)初始值
GpioDataRegs.GPASET.bit.GPIO18=1;//led 输出1

上面这样的设置   有什么问题吗?

每1s 取反一次

GpioDataRegs.GPATOGGLE.bit.GPIO18=1;

仿真时,查看MUX PUD DIR TOGGLE 寄存器都没有反应!

如果改成整个字赋值 .all=0x000001; 

就可以正常!