This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS导出dat数据头文件解释



CCS中导出的dat文件用记事本打开后头文件是这样:1651 9 40000 1 2710 2   数据保存的方式是16-unsigned,这个是什么意思呢    特别是9和2

  • 9是一个新的数据格式,2是数据长度。

    关于这个dat 文件格式的说明,终于被我找到了。网上找到的都是关于旧格式1-4的说明,这个格式9的说明只能在CCS的帮助文档中找到。

    Code Composer data file

    A text file that contains one line of header information and stores the data as one sample per line. The legacy file format supported these formats :

    • Hexadecimal

    • Integer

    • Long

    • Float

    The new scheme which is backwards compatible supports a larger set of data types. GEL_MemoryListSupportedTypes() GEL API could be used to list complete set of supported data types in the new scheme

    The header information for data files uses this syntax:

    MagicNumber  Format StartingAddress PageNum Length [NewFormat]
     
    • MagicNumber—fixed at 1651.

    • Format—a number from 1 to 4, indicating the format of the samples in the file.
      This number represents a data format: (1) hexadecimal, (2) integer, (3) long, (4) float, or (9) Use new scheme

    • StartingAddress—starting address of the block that was saved.

    • PageNum—page number the block was taken from.

    • Length—number of samples in the block.

    • NewFormat—Format (9); the new scheme. This is optional when usign the legacy formats 1 - 4

    Format 9) indicates usage of the new scheme. This was added to achieve consistency in the formats available in the memory browser and the formats available with load/save feature. The memory browser supports a larger set of data formats which vary slightly across each target. The old load/save header is based on a fixed set of data formats. In order to maintain backwards compatibility the existing fixed data format is still supported. However, an additional data format ( 9) was introduced which acts as a switch to use the new scheme. The last extra parameter (NewFormat) is the actual format chosen in the new scheme .

    All header values are assumed to be TI-style hexadecimal values.

    This is an example of a Code Composer data file:

    1651 1 800 1 10
    0x0000
    0x0000
    0x0000
    0x0000
    0x0000
    0x0000
    0x0000
    0x0000
    0x0000
    0x0000
    0x0000
    0x0000
    0x0000

    Note: Code Composer expects five-digit numbers of information to read in 4-digit values. While the data is known to be hexadecimal, Code Composer expects the  first digit to be a zero. Code Composer does this so that hexadecimal numbers beginning with letters (that is, F800) are not misread as labels. For example, when reading data in hexadecimal format from a data file, the first digit may be truncated.

    Look at this input data:

    0022
    0022
    0033
    8AC  
    FC94
    13
    895
    AB9 ...

    When reading this data, Code Composer actually reads data as:

    0022
    0033
    08AC
    0C94
    0003
    0095
    00B9 ...

    But if you test Code Composer IDE with five-digit data input, (by adding zeroes at the beginning where necessary), the output is consistent with the input:

    00022
    00033
    018AC
    0FC94
    00013
    00895
    00AB9
  • 拿UE等编辑器打开呢 显示怎么样