你好!
我用CCS3.3版本的烧写插件,怎么总出现DSP PART ID 错误。0x00EF,正确的为0x00FA,上网查了原因说是板级支持包版本不匹配,哪位有现成的?麻烦给传个好吗?找了几个不行啊,多谢了哈
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
我用CCS3.3版本的烧写插件,怎么总出现DSP PART ID 错误。0x00EF,正确的为0x00FA,上网查了原因说是板级支持包版本不匹配,哪位有现成的?麻烦给传个好吗?找了几个不行啊,多谢了哈
Qingtian,
The problem is:
The current version of the On Chip Flash Programmer does not support the device you are attempting to program. This programmer will need to be updated to obtain the newer algorithms. The updates are available in the latest Service Release and Chip Support Package available for Code Composer Studio. Updates are available with a valid subscription through the Help Menu of Code Composer Studio.
If this is the eZdsp version of CCS that was shipped with the F28335 eZdsp, it was compiled with an older version of the Flash Programmer that does not support the newer revisions of silicon. Spectrum Digital has updated this software. Please be sure to uninstall your current version first, then download the new image and install: http://support.spectrumdigital.com/ccs33/eZdsp28335_Release030320B/
Eric
你好!即是说你现在ccs的片上烧写工具不能支持你这个芯片的烧写,烧写工具需要更新。可以点击CCS的help目录下有更新选项。如果你用的CCS版本是F28335 eZdsp光碟上的软件的话,这个CCS版本是旧的版本,不支持最新的芯片,Spectrum Digital已经做出更新了,可以在下面网址去下载新的镜像
http://support.spectrumdigital.com/ccs33/eZdsp28335_Release030320B/。
另外,新的版本的CCS确实会解决这问题。建议还是下载新版本如CCSv5的调试软件,这也是以后TI主推和支持的重点。
Eric