已知输入为0-5V的电压,目前通过运算方法器将输入控制在0-3.3V的范围内,想请问如何使用28377D芯片的AD的16位差分模式?
1)因为我只有一个输入信号,如果使用12位AD应该是一路直接输入到芯片中(使用一个ADCIN引脚),差分后是不是有两路信号输入到28377D的芯片中呢(使用两个ADCIN引脚)?
2)如果16位AD是可以将一个输入信号差分为两路输入到芯片中,那么该部分的电路应该如何设计?是否有相关的例子能够提供呢?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
已知输入为0-5V的电压,目前通过运算方法器将输入控制在0-3.3V的范围内,想请问如何使用28377D芯片的AD的16位差分模式?
1)因为我只有一个输入信号,如果使用12位AD应该是一路直接输入到芯片中(使用一个ADCIN引脚),差分后是不是有两路信号输入到28377D的芯片中呢(使用两个ADCIN引脚)?
2)如果16位AD是可以将一个输入信号差分为两路输入到芯片中,那么该部分的电路应该如何设计?是否有相关的例子能够提供呢?
谢谢!
1 关于12bit的ADC,您可以看一下
e2e.ti.com/.../432547
2 关于16bit的ADC差分电路,您可以看一下
,
其使用了运算放大器 THS4531
e2e.ti.com/.../582858
If you do not provide the complimentary half of the differential signal, or if you connect the negative ADC input to ground, the ADC will simply not function correctly (you don't lose a bit).
If you have a single-ended signal that you want to sense, you should use a fully differential op-amp (e.g. THS4531) or a pair of normal single-ended op-amps to create the differential compliment about the common mode voltage (Vcm = VREFHI / 2).
Note that all voltages applied to the ADC pins should be between VSSA and VDDA at all times...differential mode of the ADC does not allow negative input voltages.
请您参考下下面的回复
https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/560613