之前我用过SDFlash3.3串口下载28016的程序,但是好像没法用这个串口烧写软件下载28069的程序,谁知道28069是否能用串口烧写程序啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前我用过SDFlash3.3串口下载28016的程序,但是好像没法用这个串口烧写软件下载28069的程序,谁知道28069是否能用串口烧写程序啊?
我看了一下您的报错,报错是说,没有反映。我目前没法用28069试,只能用28035试拉一下。
建议检查一下下面的几点:
1、28069的SCI bootload只支持• SCIRXDA on GPIO28• SCITXDA on GPIO29,您是用着两个引脚连接吗?
2、芯片有没有设定成SCI bootload模式?
3、如果以上两点你都确认,那正常的SCI和电脑通信,比如例程包中的sci_echoback能否正常运行?
4、如果上面三点都确认,那么应该能够正常烧写,codeskin就不应报错no respond。
5、如果还不行先不要用codeskin,先用串口调试助手,上电后向芯片发送41AA0800,28069应该会有返回,如果没有,那么在controlsuite中\libs\utilities\boot_rom\2806x里面有28069的bootrom源代码,你可以用仿真器监视一下。
下面是一个帖子,用的是28035,和28069都是piccolo系列,您可以参考:
http://bbs.eeworld.com.cn/thread-317887-1-1.html