现在有一个数字电源项目准备使用SYS/BIOS和28335,控制周期(也就是硬件timer的定时中断周期)为10us,由于HWI的开销太大,想使用类似non-sys/bios模式的ISR模式,TI的spraax9-Using DSP&BIOS in C2800 Applications with high Interrupt Rates.pdf文档提到这样解决办法,就是SYS/bios还是支持裸跑方式的ISR(当然不能调用OS相关的API)这个我觉得可能还有问题,因为只要跑RTOS,它在调度时都是要关中断的,而且说句实话TI SYS/BIOS的这方面优化的还需要进一步加强,他的调度时关中断的时间还是漫长的,大家可以参考:这个文章评测了DSP/BIOS的一些情况
www.netlab.tkk.fi/.../aarnikoivu_091104.pdf
因此,即便使用ISR而不是HWI,他的中断延时也是蛮大的,因此,我想知道,对于这种强实时的应用如何考虑,裸跑我认为可能比SYS/BIOS还要好一些。