This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CLA 与 CPU 数据交换的问题



28035 有两个区域CLA Shared Message RAMs,

CLA to CPU Message RAM , CLA to CPU Message RAM

我想问的是当CLA写数据到 CLA_CPU_MSGRAM 时,还没有写完,此时CPU中断读这个值,会不会出问题?

反之CPU写数据到 CPU_CLA_MSGRAM 时,还没有写完,此时CLA中断读这个值,会不会出问题?

  • Peter,

         The arbitration scheme for these registers can be found in the CLA Reference Guide. Keep in mind if the main CPU performs a read-modify-write operation on a register and between the read and the write the CLA modifies the same register, the changes made by the CLA can be lost. In general it is best to not have both processors writing to registers。

    Eric

  • Peter:

    您好!您指的是一串数组写到一半还是一个字写了几个bit?

  • 一个字写了几个bit

  • Peter,

             如果CPU和CLA同时访问一个shared RAM区域,是要遵循下面的仲裁机制的,即先后顺序,

    • CLA to CPU Message RAM: Priority of accesses are (highest priority first):
    1. CLA write
    2. CPU debug write
    3. CPU data read, program read, CPU debug read
    4. CLA data read
    • CPU to CLA Message RAM: Priority of accesses are (highest priority first):
    1. CLA read
    2. CPU data write, program write, CPU debug write
    3. CPU data read, CPU debug read
    4. CPU program read

    所以如果CLA正在写这个RAM,CPU来访问,则这时候CPU需要等。所以不会出现问题。

    Eric

     

  • 不会有问题,2000内部有自带的总线仲裁

  • 您好,Eric,

    之前您给我解答了好多问题,尤其是CLA问题,我现在又有一个cla问题,就是通过cpu.C改变cla.asm的值,我现在遇到的问题是cla.asm内的变量值可以送到cpu.c,但是通过cpu.c无法改变cla.asm的值。

    ti官网上运行28035的例程,运行cla.asm。C:\tidcs\c28\DSP2803x\v121\DSP2803x_examples\cla_adc_fir_flash

    问题:我应用的28035的例程,第一步将10赋值给_VoltFilt是对的,这是_VoltFilt等于10,在向下运行时,我设置的A4是200.375,为何_VoltFilt的不更新呢,还一直是10?

    请看:在Example_2803xClaAdcFir.c中定义:

    #pragma DATA_SECTION(A,          "CpuToCla1MsgRAM");

    float32 A [FILTER_LEN] = {62.5L, -100.25L, 200.375L, -300.25L, 10.0625L};

    在cla.asm中:

    _X4 .set _X+8
    _X3 .set _X+6
    _X2 .set _X+4
    _X1 .set _X+2
    _X0 .set _X+0

    _A4 .set _A+8
    _A3 .set _A+6
    _A2 .set _A+4
    _A1 .set _A+2
    _A0 .set _A+0

    MDEBUGSTOP
    MMOVF32 MR0,#10.6
    MF32TOUI16 MR2, MR0 ; Get back to Uint16 value
    MMOV16 @_VoltFilt, MR2

    MMOV32 MR0,@_X4 ;1 Load MR0 with X4
    MMOV32 MR1,@_A4 ;2 Load MR1 with A4
    MF32TOUI16 MR2, MR1 ;T Get back to Uint16 value
    MMOV16 @_VoltFilt, MR2 ;T
    MNOP ;3 Wait till I8 to read result