This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS28035程序下载后无法运行的问题



CCS版本为6.2  ,硬件方案采用28035内部晶振方式;外部没接晶振;TDO和GPIO34引脚为低电平,TCK\TDI\TMS接上拉电阻,cmd文件配置为FLASH存储,使用仿真器下载程序后可以正常运行,断电后再上电程序不运行;请教下,这种情况下如何判断程序上电后到底存储到FLASH中了吗,以及启动后处于的状态;

还有个问题,我在程序添加InitFLASH()函数后,程序跑飞,请问那个文档提供了关于FLASH的说明