This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377D的16bitAD,SOC0的值会串到SOC1



        如下的配置,16bit差分模式,ADC的中断是24KHZ,每24KHZ读一次AD的全部15个数据,现发现ADCA的SOC0加一个电压,ADCA的SOC1是没有加电压的,结果SOC0结果寄存器上读的值却会受到SOC1上的值影响,这是为什么呢?个人理解是SOC0切换到SOC1的过程太快,带有部分的电压值切了过去(大概这样表达),如果是这样,哪里可以配置的呢?十分紧急,谢谢

void InitAdc(void)
{
 Uint16 acqps;

 EALLOW;

    //
    //write configurations
    //ADCCLK: PRESCALE*0.5+1
    //
    AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
    AdcbRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
    AdccRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
    AdcdRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4

    AdcSetMode(ADC_ADCA, ADC_RESOLUTION_16BIT, ADC_SIGNALMODE_DIFFERENTIAL);
    AdcSetMode(ADC_ADCB, ADC_RESOLUTION_16BIT, ADC_SIGNALMODE_DIFFERENTIAL);
    AdcSetMode(ADC_ADCC, ADC_RESOLUTION_16BIT, ADC_SIGNALMODE_DIFFERENTIAL);
    AdcSetMode(ADC_ADCD, ADC_RESOLUTION_16BIT, ADC_SIGNALMODE_DIFFERENTIAL);

    //
    //Set pulse positions to late
    //1 Interrupt pulse generation occurs at the end of the conversion
    //
    AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
    AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1;
    AdccRegs.ADCCTL1.bit.INTPULSEPOS = 1;
    AdcdRegs.ADCCTL1.bit.INTPULSEPOS = 1;

    //
    //power up the ADC
    //
    AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
    AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;
    AdccRegs.ADCCTL1.bit.ADCPWDNZ = 1;
    AdcdRegs.ADCCTL1.bit.ADCPWDNZ = 1;

    //
    //delay for 1ms to allow ADC time to power up
    //
    DELAY_US(1000);

    EDIS;

    //
    //determine minimum acquisition window (in SYSCLKS) based on resolution
    //acquisition window duration is based on the System Clock,not the ADC clock(ADCCLK)
    //duration=(acqps+1)*(1/SYSCLK)
    //
 if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION)
    {
        acqps = 14; //75ns
    }
    else //resolution is 16-bit
    {
        acqps = 63; //320ns
    }

    //
    //Select the channels to convert and end of conversion flag
    //acquisition window duration is based on the System Clock,not the ADC clock(ADCCLK)
 //duration=(acqps+1)*(1/SYSCLK)
    //
    EALLOW;

    //ADCIN1P&ADCIN1N VIN-4
    AdcaRegs.ADCSOC0CTL.bit.CHSEL = 0;  //SOC0 will convert pin A0&A1
    AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps+1 SYSCLK cycles
    AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
    //ADCIN2P&ADCIN2N VIN-3
    AdcaRegs.ADCSOC1CTL.bit.CHSEL = 2;  //SOC1 will convert pin A2&A3
    AdcaRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps+1 SYSCLK cycles
    AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
    //ADCIN3P&ADCIN3N VIN-2
    AdcaRegs.ADCSOC2CTL.bit.CHSEL = 4;  //SOC2 will convert pin A4&A5
    AdcaRegs.ADCSOC2CTL.bit.ACQPS = acqps; //sample window is acqps+1 SYSCLK cycles
    AdcaRegs.ADCSOC2CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
    //ADCIN4P&ADCIN4N VOUT-2
    AdcbRegs.ADCSOC0CTL.bit.CHSEL = 0;  //SOC0 will convert pin B0&B1
    AdcbRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps+1 SYSCLK cycles
    AdcbRegs.ADCSOC0CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
    //ADCIN5P&ADCIN5N VOUT-3
    AdcbRegs.ADCSOC1CTL.bit.CHSEL = 2;  //SOC1 will convert pin B2&B3
    AdcbRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps+1 SYSCLK cycles
    AdcbRegs.ADCSOC1CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
    //ADCIN6P&ADCIN6N VIN-1
    AdccRegs.ADCSOC0CTL.bit.CHSEL = 2;  //SOC0 will convert pin C2&C3
    AdccRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps+1 SYSCLK cycles
    AdccRegs.ADCSOC0CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
    //ADCIN7P&ADCIN7N VOUT-1
    AdcdRegs.ADCSOC1CTL.bit.CHSEL = 14;  //SOC1 will convert pin C14&C15
    AdccRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps+1 SYSCLK cycles
    AdccRegs.ADCSOC1CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
    //ADCIN8P&ADCIN8N VOUT-4
    AdcdRegs.ADCSOC0CTL.bit.CHSEL = 0;  //SOC0 will convert pin D0&D1
    AdcdRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps+1 SYSCLK cycles
    AdcdRegs.ADCSOC0CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
    //ADCIN9P&ADCIN9N VOUT-M
    AdcdRegs.ADCSOC1CTL.bit.CHSEL = 2;  //SOC1 will convert pin D2&D3
    AdcdRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps+1 SYSCLK cycles
    AdcdRegs.ADCSOC1CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C

    //epwm→AD INT 4分频,SOC2
    AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 2; //end of SOC2 will set INT1 flag,看前面使用到几个SOC
    AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1;   //enable ADCINT1
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared

    EDIS;
}

//24K进入一次

interrupt void  ADCINT_ISR(void)     // ADC
{
 DINT;

     ArrayOfReceiveAdValue[SN_OF_V_IN_CH1]=(int32)AdccResultRegs.ADCRESULT0;
     ArrayOfReceiveAdValue[SN_OF_V_IN_CH2]=(int32)AdcaResultRegs.ADCRESULT2;
     ArrayOfReceiveAdValue[SN_OF_V_IN_CH3]=(int32)AdcaResultRegs.ADCRESULT1;
     ArrayOfReceiveAdValue[SN_OF_V_IN_CH4]=(int32)AdcaResultRegs.ADCRESULT0;
     ArrayOfReceiveAdValue[SN_OF_V_OUT_CH1]=(int32)AdccResultRegs.ADCRESULT1;
     ArrayOfReceiveAdValue[SN_OF_V_OUT_CH2]=(int32)AdcbResultRegs.ADCRESULT0;
     ArrayOfReceiveAdValue[SN_OF_V_OUT_CH3]=(int32)AdcbResultRegs.ADCRESULT1;
     ArrayOfReceiveAdValue[SN_OF_V_OUT_CH4]=(int32)AdcdResultRegs.ADCRESULT0;
     ArrayOfReceiveAdValue[SN_OF_V_OUT_M]=(int32)AdcdResultRegs.ADCRESULT1;

 AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
    PieCtrlRegs.PIEACK.all |= PIEACK_GROUP1;

    EINT;
}