This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何输出+/-5V的电压给THS4531供电

Other Parts Discussed in Thread: THS4531

你好,

由于目前使用的THS4531差分运算方法器需要+/-5V供电,

但是电路中只有+/-15V电源,目前是打算使用REF5050将+15V降至+5V,连接到THS4531的V+引脚。

根据REF5050的数据手册,可知REF5050的最大输入电压可为18V,那么请问我使用15V电压输入到REF5050中,输出+5V电压的方案是否可行?

-15V转为-5V目前没有什么比较好的方案,请问各位专家能否提供一种比较好的方案,最好是元器件的封装比较小一些,因为板子上的空间剩余不多了。

谢谢!