Other Parts Discussed in Thread: TMS320F28063, C2000WARE, CONTROLSUITE
关于HRCAP中断问题,
根据TI例程进行了软件配置,使用Timer0发送10KHZ的脉冲信号到HRCAP1,代码如下:
但匪夷所思的是,同样的代码,用TMS320F28063芯片,HRCAP1中断能够进去,不明白?????
#include "F2806x_Device.h"
#include "F2806x_Examples.h"
#include "F2806x_EPwm_defines.h"
#include "..\include\main.h"
#include "..\include\hw_setup.h"
#define HCCAPCLK_FREQ 120
#define HRCAP_SYSCLK_FREQ 60
#define NUM_HCCAPCLKS_PER_HCSYSCLK HCCAPCLK_FREQ/HRCAP_SYSCLK_FREQ
#define SYSCLK_FREQ 80
#define PWM1_TIMER_MIN 200
#define PWM1_TIMER_MAX 4000
#define PLL2SRC_INTOSC1 0
void HRCAP1_Config(void);
void ePWM8_Config(Uint16 period);
void Fail(void);
__interrupt void cpu_timer0_isr (void);
__interrupt void HRCAP1_Isr (void);
Uint16 first; // Count and Dly captured by 1st RISE/FALL event after cal, soft reset, or clock enable
Uint16 PULSELOW;
Uint16 PULSEHIGH=0;
Uint16 EPwm1TimerDirection;
// To keep track of which way the timer value is moving
#define EPWM_TIMER_UP 1
#define EPWM_TIMER_DOWN 0
void main(void)
{
InitSysCtrl();
InitPll2(PLL2_PLLSRC, PLL2_PLLMULT, PLL2_SYSCLK2DIV2DIS);
InitHRCapGpio();
GpioInit();
DINT;
InitPieCtrl();
// disable interrupts
IER = 0x0000; // clear interrupt enable regisger
IFR = 0x0000; // clear interrupt flag register (pending)
InitPieVectTable();
EALLOW;
PieVectTable.TINT0 = &cpu_timer0_isr;
PieVectTable.HRCAP1_INT = &HRCAP1_Isr;
EDIS;
InitCpuTimers();
StartCpuTimer0();
HRCAP1_Config(); // Configure HRCAP2 Module
//ePWM8_Config(1000);
first = 0;
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
PieCtrlRegs.PIEIER4.bit.INTx7=1;
IER|=M_INT1 | M_INT4;
ERTM;
EINT;
for(;;)
{
__asm(" NOP"); // Set breakpoint here to debug
}
}
void ePWM8_Config(Uint16 period)
{
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
EPwm8Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up
EPwm8Regs.TBPRD = 8999;
EPwm8Regs.TBPHS.all = 0x00000000;
EPwm8Regs.AQCTLA.bit.PRD = AQ_TOGGLE; // Toggle on PRD
// TBCLK = SYSCLKOUT
EPwm8Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm8Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1TimerDirection = EPWM_TIMER_UP;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
}
void HRCAP1_Config(void)
{
EALLOW;
HRCap1Regs.HCCTL.bit.SOFTRESET = 1;
HRCap1Regs.HCCTL.bit.HCCAPCLKSEL = 1; // HCCAPCLK = PLL2CLK x 2
HRCap1Regs.HCCTL.bit.RISEINTE = 1; // Enable Rising Edge Capture Event Interrupt
HRCap1Regs.HCCTL.bit.FALLINTE = 0; // Disable Falling Edge Capture Event Interrupt
HRCap1Regs.HCCTL.bit.OVFINTE = 0; // Disable Interrupt on 16-bit Counter Overflow Event
}
__interrupt void HRCAP1_Isr (void)
{
EALLOW;
if (HRCap1Regs.HCIFR.bit.RISEOVF == 1) {
ESTOP0; // Another rising edge detected before ISR serviced.
}
if (first==0) {
first = 1;
} else {
HRCap1Regs.HCCTL.bit.RISEINTE = 0;
PULSEHIGH = HRCap1Regs.HCCAPCNTFALL1 + 1;
}
HRCap1Regs.HCICLR.all = 0x001F; // Clear all HRCAP interrupts
HRCap1Regs.HCCTL.bit.RISEINTE = 1; // Re-enable rising edge interrupts
HRCap1Regs.HCICLR.bit.INT=1; // Clear HRCAP interrupt flag
PieCtrlRegs.PIEACK.bit.ACK4=1; // Acknowledge PIE Group 4 interrupts.
EDIS;
}
__interrupt void cpu_timer0_isr (void)
{
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1;
}