This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我看了下sci loopback例程里定义了以下数组
Uint16 sdataA[2]; // Send data for SCI-A
Uint16 rdataA[2]; // Received data for SCI-A
Uint16 rdata_pointA; // Used for checking the received data
然后主函数里给sdata数组写入数据
for(i = 0; i<2; i++)
{
sdataA[i] = i;
}
rdata_pointA = sdataA[0];
然后interrupt void sciaRxFifoIsr(void)就被触发了?
主要有以下疑惑:
1.sdata[]和fifo的关系是什么呢?程序里这两个好像完全没有关联,为什么给sdata写入数据后fifo就能进入中断开始发送数据呢?
2.看了下数据手册fifo的数据手册,好像并没有16个字节存放数据的FIFO寄存器,那么是怎么访问FIFO中的数据的呢?