This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSV9中导入controlSUITE的project出现问题



导入project后,还未编译就出现问题,

errors:this project was created using a version of compiler that is not currentlyinstalled-6.1.0[C2000].see'help>install new software' and select 'code generation tool updates' to check if this compiler is available through a ccs update. visit ccs app center to get the latest compiler support .or download and install the compiler,then register it with ccs through  'preferences > ccs > build > compiler'.

CCS下载的是最新版本V9-2,编译版本ti-cgt-arm_18.12.3.LTS和ti-cgt-c2000_18.12.3.LTS 。但是右击导入的project后点击properties出现的compiler version是

TI v6.1.0 ,请问怎么解决这个问题