Debugger Initialization Error
Cannot read system setup data from XML file C:\Users\ADMINI~1\WORKSP~1\EXAMPL~1\
Error parsing file:
Fatal Error at (0,0):An exception occurred! Type :RuntimeException,
message:The primary document entity could not be opened.
Id=C:\Users\ADMINI~1\WORKSP~1\EXAMPL~1\
不知是否是编译出现的warning没处理,才导致出现这个问题:
1、Invalid project path :Include path not found (\packages\ti\xdais).
2、null:creating ".sysmem" section with default size of 0x400: use the-heap
3、null:creating output section ".cio"without a SECTIONS specification
4、null:creating output section ".sysmem" without a SECTIONS specification
5、null:entry-point symbol other than "-c-int00" specified:"code-start"
6、variable "fid" was set