This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377中,同一个CMPSS的Ctriph信号与Ctripl信号能不能分别传递给trip4(假设)与trip5(假设),然后分别控制DCAEVT2与DCBEVT2?



问题背景描述如下:

cmpss3的输入信号为正弦波,设定高阈值与低阈值,一个周期之内,在高阈值以上PWM开波,低阈值以下PWM关波。我们使用CMPSS3、X-bar、Trip4、Trip5、DCAEVT2、DCBEVT2来配置。

问题描述如下:

cmpss3的CtripH和CtripL信号通过如下配置能不能分别传递Trip4和Trip5,再由Trip4和Trip5分别控制DCAEVT2和DCBEVT2,在一个周期内实现需求。

相关代码配置如下:

              EALLOW;

              //Configure DCA  to be TRIP5

                  EPwmxRegs->TZDCSEL.bit.DCAEVT2 = TZ_DCAH_HI;//011: DCAL = HI, DCAH = don't care

                  EPwmxRegs->DCTRIPSEL.bit.DCAHCOMPSEL = 0xf;             //Configure Trip5 to be DCAHCOMPSEL                                                                                              EPwmxRegs->DCAHTRIPSEL.bit.TRIPINPUT5 = 1;

              //Configure DCB  to be TRIP4

                  EPwmxRegs->TZDCSEL.bit.DCBEVT2 = TZ_DCBH_HI;//100: DCBL = high, DCBH = don't care

                  EPwmxRegs->DCTRIPSEL.bit.DCBHCOMPSEL = 0011; //Configure Trip4 to be DCBHCOMPSEL                             

                  EPwmxRegs->DCBHTRIPSEL.bit.TRIPINPUT4 = 1;  //Trip Input 4 selected as combinational ORed input to DCBL mux Reset type: SYSRSn

                  //Configure EVT2 DCA/DCB as CBC

                  EPwmxRegs->TZSEL.bit.DCAEVT2 = 1;//Enable DCAEVT2 as a CBC trip source for this ePWM module Reset type: SYSRSn

                  EPwmxRegs->TZSEL.bit.DCBEVT2 = 1;//Enable DCBEVT2 as a CBC trip source for this ePWM module Reset type: SYSRSn

              //Configure DCA/DCB path to be unfiltered & async

                  EPwmxRegs->DCACTL.bit.EVT2SRCSEL = DC_EVT2;//Source Is DCBEVT2 Signal

                  EPwmxRegs->DCACTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC;       //DCAEVT2 Force Synchronization Signal Select

                  EPwmxRegs->DCBCTL.bit.EVT2SRCSEL = DC_EVT2;                             //Source Is DCBEVT2 Signal

                  EPwmxRegs->DCBCTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC;      //DCBEVT2 Force Synchronization Signal Select*/

              EDIS;

实验结果现在是,如果DCTRIPSEL.bit.DCAHCOMPSEL这个寄存器配置成0100(即选定TRIP5),那么将得不到理论的效果,只有将其配置成0xf,才有需求的效果,但同时,DCBEVT也会触发,导致EPWMB动作,这种耦合一直存在。

如何将这两个TRIP和DCAEVT、DCBEVT分别对应起来呢?

盼望恢复,谢谢。