This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28379boot方式选择问题

之前用28335的时候,没有考虑程序引导方式的问题。最近发现,28335的四个boot选择引脚默认是内部上拉的,不接外部电路会默认选择为从flash引导。

但是到了28379这里,好像GPIO84,GPIO72这两个引脚必须要接外部上拉电路才行?希望工作人员能简单直接的讲解一下这个问题,相关技术文档查了一晚上也没有搞清楚。

多谢!

  • 您可以看一下数据手册的6.10 Boot ROM and Peripheral Booting

    The default boot mode pins are GPIO72 (boot mode pin 1) and GPIO 84 (boot mode pin 0). Users may choose to have weak pullups for boot

    mode pins if they use a peripheral on these pins as well, so the pullups can be overdriven.

    在launchpad中

    在 F2837x ControlCard 使用的是 56k weak pull-up