This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

新建的一个工程,编译时断言失败

Other Parts Discussed in Thread: CONTROLSUITE

**** Build of configuration Debug for project led ****
"D:\\ti\\ccs901\\ccs\\utils\\bin\\gmake" -k -j 4 all -O
 
Building file: "../main.c"
Invoking: C2000 Compiler
"D:/ti/ccs901/ccs/tools/compiler/ti-cgt-c2000_18.12.1.LTS/bin/cl2000" -v28 -ml -mt --include_path="D:/CCSworkspacev9" --include_path="D:/ti/ccs901/ccs/tools/compiler/ti-cgt-c2000_18.12.1.LTS/include" -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=coffabi --preproc_with_compile --preproc_dependency="main.d_raw"  "../main.c"
subdir_rules.mk:9: recipe for target 'main.obj' failed
 
INTERNAL ERROR: D:/ti/ccs901/ccs/tools/compiler/ti-cgt-c2000_18.12.1.LTS/bin/cl2000 had an internal inconsistency and aborted
                  while processing file ../main.c
 
This is caused by a defect in the TI C/C++ Compiler.
TI Customer Support may be able to suggest a workaround to avoid this.
 
Upgrading to the newest version of the compiler may fix this problem.
 
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler".  See the link titled
"Submitting an issue".
 
We need to see this ENTIRE error message and a complete, reproducible
test case including ALL of the command-line options.
 
gmake: *** [main.obj] Error 2
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
  • 你好,烦请上传一下报错内容。
    另外,根据提示应该是编译器出现了问题,可以尝试升级编译器:Help - Install new software - Code Generation Tools Updates 然后选择TI Compiler Updates中其他版本的编译器
  • 这些信息确实不好定位,如果你的CCS工具能够正常编译如controlSUITE里的例程等
    自己新建工程从最简单的开始,参考可以正常编译的例程,设置好工程属性,添加全所需源文件