This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看了TI例程 D:\ti\c2000\C2000Ware_2_00_00_03\device_support\f28004x\examples\cla cla_ex1_background_task
问题:
1、280049 的代码是否一定要运行在RAM里?为什么?
2、工程初始化代码中有如下:
void initCLA( void )
{
//
// Copy the program and constants from FLASH to RAM before configuring
// the CLA
//
#if defined(_FLASH)
memcpy((uint32_t *)&Cla1ProgRunStart, (uint32_t *)&Cla1ProgLoadStart,
(uint32_t)&Cla1ProgLoadSize );
memcpy((uint32_t *)&Cla1ConstRunStart, (uint32_t *)&Cla1ConstLoadStart,
(uint32_t)&Cla1ConstLoadSize );
#endif //defined(_FLASH)
EALLOW;
但是没定义_FLASH,而且没有在“cla_ex2_background_task_cla.cla”文件中指定 Cla1Task1()的运行位置。如果CLA代码要运行在RAM里,需要怎样配置呢?
3、如果要运行在RAM里,CMD文件需要怎样配置?
希望TI大神指点一下,谢谢!