This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WatchDog Reset问题



大家好,

我现在遇到这样的一个问题.

我做了一个28035的嵌入式Bootloader.基本功能已经实现,程序已经可以下载了,但是程序下载完成后,无法实现28035重启问题.

我做了这样的操作,

在CLK中初始化了看门狗的时钟采用外部晶振

SysCtrlRegs.CLKCTL.bit.WDCLKSRCSEL = 1; // Switch Watchdog Clk Src to external clock

看门狗采用复位方式.SysCtrlRegs.SCSR = 0x0000;

禁止看门狗复位SysCtrlRegs.WDCR = 0x0068; //disable watchdog

开始Bootloader程序.

Boot程序完成后

打开看门狗 ,并强制看门狗执行复位功能.

EALLOW;
                      SysCtrlRegs.WDCR = 0x0028;    //enable watchdog
                      SysCtrlRegs.WDCR = 0x0038;    //Reset CPU immediately
EDIS;

按照我的想法,28035应该重新启动,并根据Flash标志执行APP程序,但是现在APP并没有被执行.

而我断电重启后,系统正确执行了APP程序.

请教一下各位高人,这个复位我该如何处理.

贴上我的CMD配置.

BootLoader存放在FLASHI和FLASHBOOT.

APP中直接跳转制FLASHBOOT.

FLASH编程标志放在FLASHH


MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */

   RAML1       : origin = 0x008000, length = 0x000680     /* on-chip RAM block L0 */
   OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
   FLASHA      : origin = 0x3E8000, length = 0x004000     /* on-chip FLASH */
   FLASHB      : origin = 0x3EC000, length = 0x002000     /* on-chip FLASG */
   FLASHC      : origin = 0x3EE000, length = 0x002000     /* on-chip FLASF */
   FLASHD      : origin = 0x3F0000, length = 0x002000     /* on-chip FLASE */
   FLASHE      : origin = 0x3F2000, length = 0x002000     /* on-chip FLASD */
   FLASHF      : origin = 0x3F4000, length = 0x001FF0     /* on-chip FLASC */
   FLASHG       : origin = 0x3F5FF0, length = 0x00000F     /* on-chip FLASB */
   FLASHH       : origin = 0x3F5FFF, length = 0x000001     /* on-chip FLASA */
   FLASHI      : origin = 0x3F6000, length = 0x001800     /* on-chip FLASA */
   FLASHBOOT   : origin = 0x3F7800, length = 0x000780     /* on-chip FLASA */
   CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   CSM_PWL_PROG: origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
   
   IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */  
   IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA      /* IQ Math Tables in Boot ROM */

   ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */        
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */

PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */

   BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */  
   RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
   RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAMOS       : origin = 0x008680, length = 0x000c00     /* on-chip RAM block L0 */
   RAML2       : origin = 0x009280, length = 0x000D80
}

/* Allocate sections to memory blocks.
   Note:
         codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
                   execution when booting to flash
         ramfuncs  user defined section to store functions that will be copied from Flash into RAM
*/
 
SECTIONS
{
 
   /* Allocate program areas: */
   /* The Flash API functions can be grouped together as shown below.
      The defined symbols _Flash28_API_LoadStart, _Flash28_API_LoadEnd
      and _Flash28_API_RunStart are used to copy the API functions out
      of flash memory and into SARAM */

/******************************************************************/
/* For Piccolo B we dont need to copy the API from Flash as it is */
/* present in BOOT ROM                                              */
/******************************************************************/
Flash28_API:
   {
        -lFlash2803x_API_V100.lib(.text BootFlash)
        -lFlash2803x_API_V100.lib(.econst BootFlash)
   }                   LOAD = FLASHI,
                       RUN = RAML1,
                       LOAD_START(_Flash28_API_LoadStart),
                       LOAD_END(_Flash28_API_LoadEnd),
                       RUN_START(_Flash28_API_RunStart),
                       PAGE = 0
BootAPI:
   {
        -lrts2800_ml.lib(.cinit BootFlash)
        -lrts2800_ml.lib(.text BootFlash)
        -lExample_Flash2803x_API.obj(.cinit BootFlash)
   }                     > FLASHI        PAGE = 0




   .cinit              : > FLASHA       PAGE = 0
   .pinit              : > FLASHA       PAGE = 0
   .text               : > FLASHA       PAGE = 0
   codestart           : > BEGIN        PAGE = 0
   ramfuncs            : LOAD = FLASHI,
                         RUN = RAML1,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0

   csmpasswds          : > CSM_PWL_PROG PAGE = 0
   csm_rsvd            : > CSM_RSVD     PAGE = 0
   BootFlash           : > FLASHI        PAGE = 0
   BootProcess           : > FLASHBOOT    PAGE = 0

   /* Allocate uninitalized data sections: */
   .stack              : > RAMM0        PAGE = 1
   .ebss               : > RAMM1        PAGE = 1
   .esysmem            : > RAMM1        PAGE = 1

   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > FLASHA       PAGE = 0
   .switch             : > FLASHA       PAGE = 0

   /* Allocate IQ math areas: */
   IQmath              : > FLASHA       PAGE = 0            /* Math Code */
   IQmathTables        : > IQTABLES,    PAGE = 0, TYPE = NOLOAD
 
   /* Uncomment the section below if calling the IQNexp() or IQexp()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {
   
              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
   
   }
   */
   /* Uncomment the section below if calling the IQNasin() or IQasin()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
   {
   
              IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
   
   }   
   */

   /* .reset is a standard section used by the compiler.  It contains the */
   /* the address of the start of _c_int00 for C Code.   /*
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
   
}

///////////////////////////////////////////////////////////////////

以下部分是APP的跳转到Boot的入口方式,APP直接采用LB指令跳转到BootPrcess的地址.

    .global    _BootProcess
    .ref    _SysCtrlRegs
    .ref    _mProgramFlag
    .ref    _SCI_Init
    .ref    _Time0Init
    .ref    _fFlashProcess
    .ref    _CpuTimer0Regs
    .ref    _fInit28035
    .ref    _mReconnectTime

    .sect    "BootProcess"

_BootProcess:
    LCR    #_fInit28035
    LCR #_Time0Init
    LCR #_SCI_Init
    MOVW    DP,#_mProgramFlag
    MOVW    @_mProgramFlag,#0
    EALLOW
    MOVW    DP,#_SysCtrlRegs+25
    MOVW    @_SysCtrlRegs+25,#0x0068
    EDIS
BootContious:
    LCR #_fFlashProcess
    LB    BootContious
    NOP
    NOP
    NOP
    LRETR

  • james,

            你是用串口做bootloader来实现在线升级吗?我认为你升级完成后,可以直接使pc指针跳转到codestart的入口,或是_c_int00的入口,不一定需要复位。

             另外,看门狗初始化代码应为

             asm(" EALLOW"); 

             SysCtrlRegs.WDCR = 0x00A8;

              SysCtrlRegs.SCSR = 0x0000; //可以省略

             asm(" EDIS");

    Eric

  • Eric,

    是用串口来做Bootloader.我原来的想法是升级结束后,复位一次恢复一下28035的各种状态.codestart地址我尝试一下.

    谢谢.