This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F280049C无法连接仿真器问题



2PCS单板用仿真器连接DSP(F280049C)连接不上,错误提示:



参考TI的Debugging JTAG文档,按以下几个思路验证:

1、对比测试正常板和故障板,TCK、TDO、TMS和TDI引脚对3.3V阻抗都为4.7KΩ,对GND阻抗为5.2KΩ,排除引脚阻抗问题。

2、同一仿真器可以多次烧写正常板,故障板无法成功连接仿真器,排除仿真器问题。

3、更换仿真器烧写故障板,仍无法成功连接仿真器,排除仿真器问题。

4、DSP的复位信号正常,无跌落,排除复位信号问题。

备注:故障板在出故障前能够成功连接仿真器。

用示波器测量JTAG引脚信号,正常板和故障板TCK、TMS和TDI都为3.3V;正常板TDO为3.3V,故障板为0V,但正常板和故障板TDO引脚对VCC和GND的阻抗都一样,请问是TDO端口有问题吗?什么原因会导致TDO引脚损坏?

 附电路图: