This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377s CLA1的cmd配置



官方提供的FLASH_CLA的cmd中Cla1Prog是什么,和ramfuncs有什么区别,。如果使用#pragma CODE_SECTION来让代码在这个段编译错误提示,不能同时运行在cla和non-cla的空间呢,这个难道分配的不是cla的程序空间吗。

   Cla1Prog         : LOAD = FLASHD,
                      RUN = RAMLS5,
                      LOAD_START(_Cla1funcsLoadStart),
                      LOAD_END(_Cla1funcsLoadEnd),
                      RUN_START(_Cla1funcsRunStart),
                      LOAD_SIZE(_Cla1funcsLoadSize),
                      PAGE = 0, ALIGN(4)

可见RUN的地区是ramls5,该地址在cpu中已经初始化为cla程序空间。

为何会有这个错误提示