This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027F HALL 启动 电角度校准



工程师您好:

   我发现英文版工程师讲

For full load startup and running of zero or very low speed, you can use the hall sensor to calculate the speed and get the rotor angle, there are two ways to get the rotor angle based on hall sensor.
1. Set rotor angel to 0/60/120/180/240/300 based on hall sensor state, and use this rotor angle for Park, and I-Park modules. 
2. Calculate the rotor speed based on hall sensor state, to calculate the rotor angle by speed integral.
Both ways need to do angel offset calibration and add the angle offset to the calculated value.

同时英文工程师讲:这样校准初始角度:

Force the rotor to a zero position by setting Id to a positive value and Iq to 0, and set the angle to 0 for park module. And then check the sensing angle from the sensor.

我的问题是我在哪里设置Id  Iq?或者是我通过哪些参数来达到对Id , Iq的设置?谢谢

或者是这样,对于hall 传感器角度如何校准?

原贴地址:e2e.ti.com/.../3279266