仿真器驱动已装好,仿真器,型号选择也正确(TMS320F2809),电源正常,ccs8.3.1版本,连接目标板时提示如下错误
[Start: SEED XDS510PLUS Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\123\AppData\Local\TEXASI~1\CCS\
ti\2\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'seedjca8990isa.dll'.
The library build date was 'Apr 30 2019'.
The library build time was '14:17:18'.
The library package version is '8.1.0.00012'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
ffff 5ac3
ffff a53c
ffff 0f0f
ffff 3ca5
ffff c35a
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-342' (0xfffffeaa).
The title is 'SC_ERR_HUNG_COMMAND'.
The explanation is:
Failure due to the controller command-finish taking too long.
[End: SEED XDS510PLUS Emulator_0]
这是什么原因,怎么解决?谢谢!