This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377S的Flash Bank 0和Flash Bank 1可以整合成一块大的FLASH使用嘛

Other Parts Discussed in Thread: C2000WARE

28377S的Flash Bank 0和Flash Bank 1可以整合成一块大的FLASH使用嘛?

我看例程里面都是只用了Flash Bank 0,全部都用有需要注意或配置的地方?

  • 不可以整合成一块flash,datasheet中有一句话提到:Only one bank can be programmed or erased at a time.
    第二个问题我咨询一下美国工程师看是否有详细方法或者例程。
  • 参考一下:
    Couple of things to keep in mind while using both the banks for your application:

    1. Bank1 has an extra wait-state for fetch/read accesses. Hence, performance will be different than that of Bank0. Please map code that needs more performance

    2. Do not use the last two 128-bit (16 16-bit addresses) locations in each bank. This should already be taken care by the linker cmd files provided in C2000Ware. When Flash prefetch is enabled, if the last two 128-bit locations are used, FMC will read beyond the implemented Flash size and can end up in ITRAPs/ECC errors.

    Two banks are provided so that needed customers can use one of them for code and one for data. Also, users can maintain two images if they want for firmware upgrade reasons.