This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急 非常急 MSP432 程序下载不了 用的是CCS9.3



你好  我用MSP432P401R 开发项目,昨天还是能下载连接成功,

今天就不能连接了,前期我用的是MSP-EXP432P401R  开发板写程序的

具体见word 附件非常急 MSP432开发板连接不上CCS.docx

  • 1 您可以先尝试一下对芯片执行恢复出厂设置MSP432_Factory_Reset,参考下面链接内第5章FAQ内给出的步骤

    www.ti.com/.../slau597f.pdf

    Q: I can't program my LaunchPad development kit; the IDE can't connect to target. What's wrong?

    2 您是否可以确认设备上的芯片不是XMS芯片,并且设备版本是C还是D?
  • 根据word文档的提示你用的是XMS432P401R,是官方的那个小黑板吧。这个是以前的版本,你应该是升级了xds110的固件,最新的固件是不支持的,比较悲剧。解决办法是降级,可以找找我在TI论坛的评测文章,里面有办法,当然最好是换最新的小红板使用,不要用小黑板了。
  • 你好 工程师 我用的是小红板,上几天 一直在用 都是可以的 XDS 110 2PIN模式
    帮忙分析一下其他原因
  • 请您对芯片执行恢复出厂设置MSP432_Factory_Reset 看结果如何,谢谢
  • Susan Yang   你好

    1、按你提供的方法 进行测试,发现不行,本来就不能连接,想通过CCS 来进行对对芯片执行恢复出厂设置MSP432_Factory_Reset,......发现是不行的。

    CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)  No connection possible. This could be caused by the device having gone to low power mode and disabling JTAG PINs. You have the option to either toggle reset or try to use SWD instead.

    MSP432_Factory_Reset() cannot be evaluated.

    Could not write register DP_RESET: target is not connected

    at DP_RESET=1 [msp432_factory_reset.gel:44]

    at MSP432_Factory_Reset()CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)  No connection possible. This could be caused by the device having gone to low power mode and disabling JTAG PINs. You have the option to either toggle reset or try to use SWD instead.

    CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)  No connection possible. This could be caused by the device having gone to low power mode and disabling JTAG PINs. You have the option to either toggle reset or try to use SWD instead.

    2、最新版本和你给的文档  说法不一样。

    这里 我选的是2PIN ,在上个文档里已说了

    3、我用的就是从网上买的demo板 ,并且原来都能工作的。不用怀疑芯片型号

    4、帮忙找个专家会诊一下,TI的开发 就是各种坑 ,希望你们能给个有限的方法。急急

  • 很抱歉,我现在无法看到您的图片,请您重新上传一下

    您是在何处购买的?
  • 就是二层的小红板

  • 目前我们在美国开发项目、在digkey网站上购买的
  • 关于错误Error -1170 @ 0x0

    我们有一个专门的说明

    software-dl.ti.com/.../ccsv7_debugging_jtag_connectivity_issues.html

    此错误是由JTAG调试器无法访问DAP或其ARM子核心之一引起的。这通常是由于主板上的硬件故障或子核心上的无效代码(导致其不断重置自身)引起的。

    如果此错误是由软件引起的,则可以通过直接访问DAP并尝试通过GEL脚本尝试重置有问题的内核,对其进行锁定或擦除其闪存来恢复该错误(某些微控制器已预先加载了例程以允许该错误) 。

    另外对于所有使用XDS110调试探针的启动板,最近的默认TCLK速度更改可能会导致此问题。请检查JTAG Clock speed considerations

    software-dl.ti.com/.../emu_xds110.html
  • 给出的方法 ,真心没有任何价值,TI做的就是反人性,把本来很简单的做到非常复杂,其他友商 2个pin就解决了,ti 非要整出一堆问题
  • 即使你是小红板,还是XMS的芯片,我认为不支持太高的xds110的版本,降级试试CCS7.x的版本。

  • 客户已经在下面的帖子分享了板子的图片

    e2echina.ti.com/.../571177

    是REV 2.1版本的小红板