This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好,我用FLASH API对F28377D进行FLASH烧写,只烧写E扇区(0x88000开始),其他扇区没动,把代码烧写进去后,在仿真器中,我选择CPU RESET后,调试窗口提示:“Break at address "0x3ff16a" with no debug information available, or outside of program code.”
运行,调试窗口又提示 "Break at address "0x3fe443" with no debug information available, or outside of program code."
打开汇编指令看,这个位置是 “ESTOP0” 指令。
然后,我又断电后重新,发现软件运行还是不正常。
请问,这个问题怎么解决???? 谢谢!
谢谢!
已经解决了。
oReturnCheck = Fapi_issueProgrammingCommand((Uint32 *)(Flash_Address),Buffer,Buffer_Counter, 0, 0, Fapi_DataOnly);
这个函数的参数我使用错了,必须用:
oReturnCheck = Fapi_issueProgrammingCommand((Uint32 *)(Flash_Address),Buffer,Buffer_Counter, 0, 0, Fapi_AutoEccGeneration);