This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-C2000EVM中的TDC芯片的LNA以及PGA对弱信号的衰减作用问题

       最近运用TDC1000-C2000EVM这个开发板的时候,采用信号源输出连续正弦波信号S1,模拟接收探头收到的输入回波信号,测试开发板的链路CH2接收通道中LNA以及PGA对弱信号的增益能力时,发现LNA以及PGA不但没有放大信号,反而使信号发生了衰减,如果旁路掉LNA以及PGA,则对信号的幅值没有影响。

 S1的参数为:20mVPP,200KHz,offset为1.65V,如图所示:

将这个信号连接到开发板的J5的11引脚。将开发板GUI的通道配置为CH2,使用片上时钟8MHZ,在分频选项设置为4分频,以便与输入信号200K匹配。

使用示波器探头对开发板上TDC芯片U1的Pin2引脚也就是RX2接收端进行测量,可以看到信号经过电容C4以后的峰峰值为16mV(图中蓝色信号)。

此时将GUI里的LNA配置为Active状态,用示波器探头对R21近LNAOUT端进行测量,可以发现信号此时峰峰值为11.6V,

如果将GUI里面的LNA旁路掉(即bypass选项),会发现LNAOUT值变回16mV,说明旁路LNA时,则对信号没有衰减。连续多次测量,此规律不变,说明在使能LNA时,对信号并没有增益,反而发生了约30%的衰减。

将LNA保持在Active状态,对U1的Pin5引脚也就是PGAIN的输入进行测量可以看到信号的峰峰值为11.4mVpp.

将GUI里的GNA配置为Active状态,PGA-GAIN设置为21DB增益,对R27靠近PGAOUT端进行测量,可以发现信号此时峰峰值为5.8mVpp,

更改PGA-GAIN的值为9DB,对R27靠近PGAOUT端进行测量,可以发现信号此时峰峰值为8mVpp,

持续对PGA-GAIN的值进行调整可以发现该值越大,对信号的衰减越强。如果将PGA旁路掉(即bypass选项),会发现GNAOUT值为11.2mVpp。说明PGA对信号也发生了衰减,并且衰减程度随着PGA-GAIN值的增大而变得更强。

如果将GUI中的LNA 以及PGA都选为bypass选项,可以发现R21靠近LNAOUT端以及R27靠近PGAOUT端的信号值与其对应的输入值幅度并没有发生明显的衰减。

按照开发板的设计初衷,信号幅值经过LNA 以及PGA的时候本来应该被放大的,但是为什么此时LNA和PGA反而将信号衰减了呢,请教一下TI方的技术人员,以及其他各位大神指教为什么会这样,谢谢。