在C2000里面看到很多工程都是用的这个延时函数,请问在哪里可以找到它的源代码,或者在哪个.h文件。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在C2000里面看到很多工程都是用的这个延时函数,请问在哪里可以找到它的源代码,或者在哪个.h文件。谢谢
//***************************************************************************** // //! Delays for a fixed number of cycles. //! //! \param count is the number of delay loop iterations to perform. //! //! This function generates a constant length delay using assembly code. The //! loop takes 5 cycles per iteration plus 9 cycles of overhead. //! //! \note If count is equal to zero, the loop will underflow and run for a //! very long time. //! //! \return None. // //***************************************************************************** extern void SysCtl_delay(uint32_t count);
在 sysctl.h 内