This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

motorware 工程使用问题

Expert 1119 points
Other Parts Discussed in Thread: DRV8301

选用DRV8301_69M套件,用lab3a工程,填入自己的参数,可以控制转速,不过,我想知道,电流随着转速升高而加大,是不是到一定程度电流就不再加大了?

我的情况是:转速1K时候0.8A;2K时候1.6,加大到4K,电流3.4A,再加大转速,电流没啥变化。我的电机(压缩机)是空载。

不过据同事说,在有负载情况下,电流也到不能加大了。这导致负载有点带不动啊。我们成型的产品,到4K转速时候电流能到7A左右。我读取程序中的转速值,的确是4000转到了。请问这是软件问题还是硬件问题呢?是不是我选的工程不太合适?