This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

鸵鸟蝈蝈进,求助



您发给我的这个文件里,第3页有这样一段话:

TMS320F2806x系列Picolo DSP可在CCS3.3下仿真,但片内Flash的烧写须在CCS4.2以上版本中
执行,因此若使用TMS320F2806x系列的DSP,推荐使用CCS4.2,仿真器推荐使用
TDS510Plus、TDS560Plus

现在问题是:我用的SEED的仿真器,是否也支持TMS320F2806x系列Picolo DSP在CCS3.3下仿真?

还一个是,为啥TMS320F2806x能在CCS3.3下仿真,烧写需在CCS4.2以上版本中?在CMD中配置到FLASH里,代码不会烧进FLASH?谢谢

7485.CCS3.3中28069配置.pdf
  • SEED的仿真器我没有用过,理论上讲也可以。通过修改28035的cmd文件,编译器可以编译28069的代码。

    CCS3.3的烧写插件不支持F28069。

    推荐使用CCS5。。。。

  • 仿真是在上电情况下将程序load到RAM上运行(掉电后即丢失),而不是烧写在Flash里,要实现烧写,需要调用FlashAPI将Flash里的程序擦除(Erase),烧用户程序写入(Program),然后进行校验(Verify),而这些动作本身也需要程序来运行,楼上提到的烧写插件就是实现这些功能的,但v3.3下并没有集成它,只有之后推出的v4/5才可以实现。