CCS中添加例程:C2000Ware_MotorControl_SDK_3_00_00_00/solutions/boostxl_3phganinv/f2837x,烧写过程出错,cpu1 与cpu2的.out文件怎么添加??步骤是怎样 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CCS中添加例程:C2000Ware_MotorControl_SDK_3_00_00_00/solutions/boostxl_3phganinv/f2837x,烧写过程出错,cpu1 与cpu2的.out文件怎么添加??步骤是怎样 ?
我刚刚又测试了一次,把该例程的.out文件载入cpu1,然后运行程序,VA、VB、VC还是得不到任何输出。下图是我的debug图。 有时还会报如下错误:Trouble Removing Breakpoint with the Action "Finish Auto Run" at 0xdb74: (Error -1066 @ 0xDB74) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 8.1.0.00005)。 刚入手这块板子,还是有不少问题解决不了,感谢您耐心的解答
关于此错误,默认情况下,调试器在调试过程中会自动设置一些断点。一个在“主程序”处,另一个在程序的退出点处。程序加载后,它将尝试在“ main”处设置一个断点并对其自动运行。可以在调试器属性中禁用此行为:
https://processors.wiki.ti.com/index.php/Debug_Handbook_for_CCS#Auto_Run_and_Launch_Options
目前手边只有一个28379的LAUNCHPAD,没有上面的小绿板,所以无法为您直接测试程序输出
强烈推荐您参考一下文档C:\ti\c2000\C2000Ware_MotorControl_SDK_3_00_00_00\solutions\boostxl_3phganinv\docs下的
sluubp1a_BOOSTXL-3PhGaNInv Evaluation Module User Guide (Rev. A)
中的
2.4.2 Set up BOOSTXL-3PhGaNInv EVM Board Specific Project With Code Composer Studio™ (CCS)Software
谢谢你的答复。目前,我只有28379d和boostxl-3phganinv在手,对于双电机例行程序,我没有马达。我想测试一下小绿板逆变是否能完成,希望在示波器上可以检测正弦波。根据我目前的情况,我能进行这项操作吗?是否需要将Va,Vb,Vc接负载,然后测量相电流?
或者根据我在28379d中编写的SVPWM程序,测试boost xl-3phganjnv的逆变性能,想测试得到正弦波,可以实现吗?