This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28379D Vienna CCS7.4



Ti Team,

你好,我现在购买了Vienna Demo板加28379D的核心板进行原理研究,

关于Vienna 调试问题点需要确认:

  1. 开发板的功率板市电N与BUS N是断开的(Cm1),需不需要连接到一起?
  2. 调试Vienna开发板需要适配多大的调压器?120Vrms, 50Hz的工作条件是否影响正常工作?
  3. 在CCS程序里,找不到AD转化后再转回实际值的过程,这个是怎么处理的?
  4. 三相市电不平衡,是不是可控?对测试流程是不是有影响?
  5. 市电电阻电压采样,没有发现用途这个是做预留么?
  6. PWM波输出A/B 2路信号一样,程序只初始化了COMPA,死区没有进行配置(默认EPWMA从比较器A输出,EPWMB从比较器B输出),我没有找到从影子寄存器A可以同时加载数值到COMPA和COMPB,这个是什么原因?