This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dsp的分页机制



对于dsp28335,程序的寻址空间为4M,数据寻址空间是4G。当程序大于4M时,则意味着程序空间不够,在实际中采用分页机制,可以扩展实际的寻址空间。

1、由于28335采用的是程序和数据统一编址,分页就相当于把程序的4M分为一个页,如何数据的4M分为第二页,由于程序空间大小就4M,因此后面所有的页全是数据的?

2、分页机制为什么可以扩展实际的寻址空间,28335采用的哈弗结构,数据和程序是分开存储,数据空间中是不能存放程序,当程序大于4M时,如何通过分页实现地址扩展?

该部分内容为手把手教你学DSP28335中的第62面产生疑问