TI E2E™ 设计支持论坛将于 5 月 30 日至 6 月 1 日进行维护。如果您在此期间需要技术支持,请联系 TI 的客户支持中心寻求帮助。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于F2837D的CMD文件中的FPUmathTables段定义问题

Other Parts Discussed in Thread: C2000WARE

编译显示以下警告信息

Description Resource Path Location Type
#10247-D creating output section "FPUmathTables" without a SECTIONS specification PMSM_FOC_F28379D_LEGACY_CPU1 C/C++ Problem

未在2837xD_RAM_lnk_cpu1.cmd文件中发现FPUmathTables段的段定义,也未在c2000 ware中发现F28379D的FPUmathTables段定义;

1) 这个段定义具体到F28379D的cmd文件中,应该如何定义?按照本人理解,FPUmathTables应该是一段固化的查找表,类似于IQmathTables,应该是对应具体芯片的内存地址,但是在F28379D的数据手册中未找到该段地址,

2)该段定义的起始地址和段长应该定义为多少?还是随便给一段空间分配段定义?

  • 您可以参考下面的代码,路径为C:\ti\c2000\C2000Ware_3_01_00_00\libraries\dsp\FPU\c28\examples\common\f2837xd

    例程路径为 C:\ti\c2000\C2000Ware_3_01_00_00\libraries\dsp\FPU\c28\examples\fft\2837x_rfft_adc

    //#############################################################################
    //
    // FILE:    F2837xD_FPU_RFFT_ADC_lnk.cmd
    //
    // TITLE:   Linker Command File for FPU library examples that run 
    //          on the 2837x platform
    //
    //          This file includes all RAM and FLASH blocks present on the
    //          2837x and depending on the active build configuration(RAM or FLASH)
    //          the appropriate sections will either be loaded into RAM or FLASH 
    //          blocks
    //
    //#############################################################################
    // $TI Release: C28x Floating Point Unit Library V2.03.00.00 $
    // $Release Date: Mar 19, 2020 $
    // $Copyright: Copyright (C) 2018 Texas Instruments Incorporated -
    //             http://www.ti.com/ ALL RIGHTS RESERVED $
    //#############################################################################
    // NOTES:
    // 1. In addition to this memory linker command file, add the header linker 
    //    command file directly to the project. The header linker command file is 
    //    required to link the peripheral structures to the proper locations within
    //    the memory map.
    //    
    //    The header linker files are found in 
    //    c2000\C2000Ware_X_XX_XX_XX\device_support\f2837x(d/s)\headers\cmd
    //    
    //    For BIOS applications add:      F2837x(D/S)_Headers_BIOS_cpuX.cmd
    //    For nonBIOS applications add:   F2837x(D/S)_Headers_nonBIOS_cpuX.cmd
    //
    // 2. On reset all RAMGSx blocks are under the mastership of CPU1. The user
    //     must configure the appropriate control registers to transfer mastership
    //     of a RAMGSx block over to CPU2
    //
    // 3. Memory blocks on F2837x are uniform (ie same physical memory) in both 
    //    PAGE 0 and PAGE 1. That is the same memory region should not be defined 
    //    for both PAGE 0 and PAGE 1. Doing so will result in corruption of program
    //    and/or data.
    //    
    //    Contiguous SARAM memory blocks can be combined if required to create a 
    //    larger memory block.
    //
    //#############################################################################
    
    // The following definitions will help to align the input buffer.For the complex FFT
    // of size N, the input buffer must be aligned to a 4N word boundary. For a real FFT
    // of size N, the input buffer must be aligned to a 2N word boundary. The user may define
    // the macro either in the linker command file, as shown here, or
    // through the project properties under,
    // C2000 Linker -> Advanced Options -> Command File Preprocessing -> --define
    --define RFFT_ALIGNMENT=1024
    #if !defined(RFFT_ALIGNMENT)
    #error define RFFT_ALIGNMENT under C2000 Linker -> Advanced Options -> Command File Preprocessing -> --define
    #endif
    
    MEMORY
    {
    PAGE 0 :
       /* BEGIN is used for the "boot to SARAM" bootloader mode   */
    #if defined(RAM)
       BEGIN           : origin = 0x000000, length = 0x000002
    #elif defined(FLASH)
       BEGIN           : origin = 0x080000, length = 0x000002
    #endif 
       RAMM0           : origin = 0x000122, length = 0x0002DE
       RAMM1           : origin = 0x000400, length = 0x000400
       
       RAMD0		   : origin = 0x00B000, length = 0x000800
       RAMD1		   : origin = 0x00B800, length = 0x000800
       
       RAMLS0          : origin = 0x008000, length = 0x000800
       RAMLS1          : origin = 0x008800, length = 0x000800
       RAMLS2          : origin = 0x009000, length = 0x000800
       
       RAMGS0		   : origin = 0x00C000, length = 0x001000
       RAMGS1		   : origin = 0x00D000, length = 0x001000
       RAMGS2		   : origin = 0x00E000, length = 0x001000
       RAMGS3		   : origin = 0x00F000, length = 0x001000
       
       RESET           : origin = 0x3FFFC0, length = 0x000002
       
       FLASHA           : origin = 0x080002, length = 0x001FFE	/* on-chip Flash */
       FLASHC           : origin = 0x084000, length = 0x002000	/* on-chip Flash */
       FLASHD           : origin = 0x086000, length = 0x002000	/* on-chip Flash */
       FLASHE           : origin = 0x088000, length = 0x008000	/* on-chip Flash */
       FLASHF           : origin = 0x090000, length = 0x008000	/* on-chip Flash */
       FLASHG           : origin = 0x098000, length = 0x008000	/* on-chip Flash */
       FLASHH           : origin = 0x0A0000, length = 0x008000	/* on-chip Flash */
       FLASHI           : origin = 0x0A8000, length = 0x008000	/* on-chip Flash */
       FLASHJ           : origin = 0x0B0000, length = 0x008000	/* on-chip Flash */
       FLASHK           : origin = 0x0B8000, length = 0x002000	/* on-chip Flash */
       FLASHL           : origin = 0x0BA000, length = 0x002000	/* on-chip Flash */
       FLASHM           : origin = 0x0BC000, length = 0x002000	/* on-chip Flash */
       FLASHN           : origin = 0x0BE000, length = 0x002000	/* on-chip Flash */   
    
    
    PAGE 1 :
       BOOT_RSVD       : origin = 0x000002, length = 0x000120     /* Part of M0, BOOT rom will use this for stack */
    
       RAMLS3          : origin = 0x009800, length = 0x000800
       RAMLS4          : origin = 0x00A000, length = 0x000800
       RAMLS5          : origin = 0x00A800, length = 0x000800
       
       RAMGS45		   : origin = 0x010000, length = 0x002000
       RAMGS67		   : origin = 0x012000, length = 0x002000
       RAMGS89		   : origin = 0x014000, length = 0x002000
       RAMGS1011	   : origin = 0x016000, length = 0x002000
    
       RAMGS12		   : origin = 0x018000, length = 0x001000
       RAMGS13		   : origin = 0x019000, length = 0x001000
       RAMGS14		   : origin = 0x01A000, length = 0x001000
       RAMGS15		   : origin = 0x01B000, length = 0x001000
    
       FLASHB          : origin = 0x082000, length = 0x002000	/* on-chip Flash */
       
    }
     
    SECTIONS
    {
       codestart        : > BEGIN,     PAGE = 0
    #if defined(RAM)
       .TI.ramfunc      : > RAMM0,     PAGE = 0
       .text            :>> RAMM1 | RAMD0 | RAMD1 | RAMLS0,  PAGE = 0
       .cinit           : > RAMLS1,    PAGE = 0
       
       .pinit           : > RAMLS1,    PAGE = 0
       .switch          : > RAMLS1,    PAGE = 0
       .econst          : > RAMLS4,    PAGE = 1
    #elif defined(FLASH)
       .TI.ramfunc      :  LOAD = FLASHC,
                           RUN = RAMLS1,
                           RUN_START(_RamfuncsRunStart),
                           LOAD_START(_RamfuncsLoadStart),
                           LOAD_SIZE(_RamfuncsLoadSize),
                           PAGE = 0
    
       .text            : > FLASHN,    PAGE = 0
       .cinit           : > FLASHM,    PAGE = 0
    
       .pinit           : > FLASHM,    PAGE = 0
       .switch          : > FLASHM,    PAGE = 0
       .econst          : > FLASHB,    PAGE = 1
    #else
    #error Add either "RAM" or "FLASH" to C2000 Linker -> Advanced Options -> Command File Preprocessing -> --define
    #endif //RAM
    
       /* Test specific sections */
       RFFTdata1        : > RAMGS45,   PAGE = 1, ALIGN = RFFT_ALIGNMENT
       RFFTdata2        : > RAMGS67,   PAGE = 1
       RFFTdata3        : > RAMGS89,   PAGE = 1
       RFFTdata4        : > RAMGS1011, PAGE = 1
       
       FPUmathTables    : > RAMGS12,   PAGE = 1
       
       .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
    
       .cio             : > RAMLS3,    PAGE = 1
       .sysmem          : > RAMLS3,    PAGE = 1
    
       .stack           : > RAMLS4,    PAGE = 1
       .ebss            : > RAMLS5,    PAGE = 1
       .esysmem         : > RAMLS4,    PAGE = 1
         
    }
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

  • 好的,谢谢您!看起来FPUmathTables 的段存储空间定义也是随机指定的RAMGS12内存片,不是像之前的28335一样指定一块固定的RAM存储区域