This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

280049 ADC Conversion Priority 中第二种优先级方式问题



各位好!

我针对ADC Conversion Priority章节(13.7)中的第二种优先级方式有不明白的地方,请大家帮我看看,谢谢!

具体如下:

High priority mode is assigned first to SOC0, then in increasing numerical order这句描述的意思是否是这样,例如现在向SOCPRIORITY中写了4,表示SOC0~SOC3是高优先级,其中SOC0优先级最高,然后最高优先级会依次传递给SOC1,SOC2和SOC3。例如现在SOC1的优先级最高,那么当SOC0和SOC1同时收到触发时,SOC1会先转换。

如果我的理解没错,那么是否与这句描述矛盾If two high priority SOC’s are triggered at the same time, the SOC with the lower number will take precedence?这句描述的应该是无论什么时候,SOCPRIORITY中写了4后,SOC0~SOC3中序号小的优先级最高。