This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

无法连接目标板,在Target Configuration File配置页面的Test Connection之后出现如下结果。

最新的Test Connection结果如下:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\DOCUME~1\ADMINI~1\LOCALS~1\APPLIC~1\.TI\
4084209646\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'seedjca8990isa.dll'.
The library build date was 'Oct 3 2012'.
The library build time was '21:58:41'.
The library package version is '5.0.872.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '1' (0x00000001).
The controller has an insertion length of '16' (0x00000010).
This utility will attempt to reset the controller.

A error occurred while attempting to reset the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-342' (0xfffffeaa).
The title is 'SC_ERR_HUNG_COMMAND'.

The explanation is:
Failure due to the controller command-finish taking too long.

[End]

仿真器是seed的XDS510,虽然Test connection结果是failure但是当我点击debug的时候程序是可以进行调试的。

问这样会带来什么影响呢?

对最终程序固化进28035有影响吗?