Other Parts Discussed in Thread: UNIFLASH
使用的CCS9.2.0,控制芯片为28335,使用XDS100V3可以正确连接仿真器。当仿真器换成XDS560V2PLUS时,仿真器连接失败,测试结果如下:
[Start: SEED XDS560V2 USB Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\zhm23\AppData\Local\Texas Instruments\
CCS\ccs920\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'seed560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_conf
Download failed for file E:\Program Files\ti\ccs920\ccs\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
[End: SEED XDS560V2 USB Emulator_0]
希望各位大神能指点迷津,万分感谢!!!