我用280049 的HRCAP功能,采样和校准中断都放在cla中处理。我把task1设置为ecap的4个边沿触发事件中断,进中断的频率大概500khz,task2任务设置成校准,大概1.6ms触发一次。运行仿真发现,task1正常响应和处理而task2一直不能进入。我的问题 是不是因为task1优先级高,执行频率高,但task2中断被忽略?当我把task1和task2任务的函数对换,两个都能正常工作了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用280049 的HRCAP功能,采样和校准中断都放在cla中处理。我把task1设置为ecap的4个边沿触发事件中断,进中断的频率大概500khz,task2任务设置成校准,大概1.6ms触发一次。运行仿真发现,task1正常响应和处理而task2一直不能进入。我的问题 是不是因为task1优先级高,执行频率高,但task2中断被忽略?当我把task1和task2任务的函数对换,两个都能正常工作了。
谢谢 已经通过timer测量出task的执行时间。debug模式仿真c28程序可以使用clock测量执行时间,当仿真CLA时clock无效,我使用的软件版本是CCS9.3.0