This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL F28379D开发板烧写FLASH无法运行

Other Parts Discussed in Thread: TMDXIDDK379D

目前使用LAUNCHXL F28379D开发板,烧写例程fcl_f2837x_tmdxiddk,ram运行没问题,flash烧写后点运行没问题,但是掉电后重启,程序没有运行!

我尝试过论坛的方法,比如flash烧写成功后,不允许直接退出再掉电,但是上电后仍然运行不了!

板子上的Boot开关默认为111.

  • 我们会在测试后给您回复
  • Ti的例程我什么都没改动,Properties里面直接把ram设成flash,set Flash active,然后烧写,在线跑没问题,断电重启就不跑了,我通过LED闪烁来判断的!这个问题困扰我三天了,麻烦尽快解决!也就是Ti例程,改成flash烧写,需要软件比如cmd做哪些改动,Configure需要哪些改动!我试了dual-axis_serve_drive_fcl_qep_f2837x例程,也是一样的效果!
  • 很抱歉,回复有些晚了

    您可以检查板上的启动boot模式选择开关以确保将其设置为flash吗?应该为011

    具体可以看一下Table 4-4. Device Default Boot Modes for CPU1

    www.ti.com/.../spruhm8i.pdf

    另外该示例是针对F2837x controlCARD和TMDXIDDK379D板的。您需要编辑代码以使其可以在LaunchPad上使用