This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PWM1_H给脉冲其余都关断的话测量电压

Other Parts Discussed in Thread: MOTORWARE

28335电机套件仅给PWM1_H,其余信号关断,只能采集到U相电压为12V,这是为啥呢

  • 采集U相对地电压是12V
  • 你好,你说的“仅给PWM1_H,其余信号关断”是指只使能PWM1吗?采集到的U相电压是用示波器还是电压表采集的?
  • 是给PWM1H一个占空比为50%的PWM信号,其余的不给信号,也不连接电机。然后用示波器测量U对地电压。这样做的目的是在参数识别的时候需要给电机UV通直流脉冲,但是这个直流脉冲时间不能过长,否则会过流,仅仅这一瞬间很难测得电压。所以在不连接电机的情况下,先测量U的电压是否符合理论情况,然后再连接电机。但是测量的电压是12V,这显然和想象的不太一样。
  • 是给PWM1H一个占空比为50%的PWM信号,其余的不给信号,也不连接电机。然后用示波器测量U对地电压。这样做的目的是在参数识别的时候需要给电机UV通直流脉冲,但是这个直流脉冲时间不能过长,否则会过流,仅仅这一瞬间很难测得电压。所以在不连接电机的情况下,先测量U的电压是否符合理论情况,然后再连接电机。但是测量的电压是12V,这显然和想象的不太一样。
  • 如果将PWM占空比设置为50%,并且套件未损坏,则在U / V / W上应该看到相同的信号。您可以对motorWare中的高压套件使用lab01或lab01b进行验证。
    另外,电压12V是什么意思?是一个直流的12V信号吗?
  • 我是说只给PWM_1H信号,不给另外五个桥臂信号的情况下,您回复的也是这个情况吗?我看了下lab01b的说明书上好像是三相信号,您的意思是让我屏蔽掉其他五个信号进行验证吗?
    12V电压是一条平线,大小12v